38.5.10 Aborting Transmission
A pending transmission can only be aborted before the transmission of the message starts, before the Start-of-Frame (SOF).
The transmission of a specific FIFO can be aborted by clearing TXREQ in the
CAN Transmit Queue Control register; it cannot be aborted by clearing the bits in the
CxTXREQ registers. Writing a ‘0
’ to one of the bits in the CxTXREQ
registers will be ignored. The TXABT bit in the CAN FIFO Status y register will be set
after a successful abortion. TXREQ will remain set until the message either aborts or is
successfully transmitted.
Setting ABAT (CxCON[27]) will abort all pending messages of all FIFOs. After all TXREQx bits are cleared, ABAT has to be cleared in order to transmit new messages.
Clearing TXREQ for a transmit FIFO will attempt to abort all transmissions in the FIFO. If a message is successfully transmitted, the FIFO index will be updated as normal. If the message is successfully aborted, the FIFO index will not change.
The user can then use the FIFO Message Index bits, FIFOCI[4:0] (CxFIFOSTAy[12:8]), to identify messages that are transmitted. To reset the transmit FIFO index and erase all pending messages, the user can set the FRESET bit. The FIFO can then be loaded with new messages to be transmitted.