3.1 CryptoAuth Trust Platform Connections
The 3-Lead Contact mikroBUS Socket Board has dedicated SWI and SWI-PWM connections through the mikroBUS header that enable it to connect to the mikroBUS host header present on the Trust Platform or any of the PIC/AVR/SAM MCU host development boards that have a mikroBUS header. Both SWI and SWI-PWM connections are always connected to the host micro on the Trust Platform board.
Connecting the 3-Lead Contact mikroBUS Socket Board to the CryptoAuth Trust Platform
- Configure the EV27Y72A to the desired mode as specified in Modes of Operation.
- Set the switches on the
CryptoAuth Trust Platform to disable the on-board devices. Note that the SW2_1
switch will have no effect on this mikroBUS board. This setting is highlighted
in bold and italic below:
Switch Settings What is Enabled SW2_1 SW2_2 mikroBUS™ Header On-Board Devices N/A ON Yes Yes N/A OFF Yes No - Connect the two boards as shown
in the following figure.
Figure 3-1. EV27Y72A Connected to a CryptoAuth Trust Platform Development Board
Remember: The angled notch on the 3-Lead Contact mikroBUS Socket Board must be aligned with the angled line on the silk screen near the mikroBUS connector. - Connect a USB cable between the CryptoAuth Trust Platform on the host system where the software is developed.
- Invoke the software tools for the given application or the use case that is being developed.