4 Installing the MPLAB® Code Configurator Melody CAN-TP Library
The following instructions describe how to install the MCC plugin and the CAN-TP Library in MPLAB X IDE.
To install the MPLAB® Code Configurator Plugin:
- In MPLAB X IDE, select Plugins from the Tools menu
- Select the Available Plugins tab
- Check the box for the MPLAB® Code Configurator and click on Install
To install the CAN-TP Library:
- Open MCC in MPLAB® X
- In the MCC Content Manager Wizard window, select the Content Type to be MCC Melody
- Under Optional Content, go to Optional Content → Libraries
- Tick the box next to CAN-TP and Click Finish
- In the Content Manager window, select the latest version or the perferred version of the Library and click Apply