4.3.4 Operation on IB (Information Block) File

Figure 4-18. MCHPRT3 PIC32-BZ6 GUI for IB (Information Block) File Operation

The user can perform the following in the IB File tab:

  • Read the IB(1) File to IB Buffer(2).
  • Save IB Buffer into the IB File.
  • From the “IB Type” drop-down list, select Flash (default value).
  • Read the IB from DUT into the IB Buffer.
  • Commit the IB Buffer into DUT—the IB is stored in the Flash.
Note:
  1. Use the Information Block (IB) to store various types of calibration and system configuration information.
  2. The IB Buffer is a temporary PC location for the Information Block (IB).