4.3.3 Calibration Flow Demonstration
In this demonstration, the user can calibrate TX parameters and RX parameters of the PIC32-BZ6 using a PC with the installed MCHPRT3 tool. The calibration step could be checked in the “Cal. Flow Status” in the Calibration page.
Perform the following steps for the demonstration of the calibration flow (see the following figure):
- Set up the connection between the PIC32-BZ6 Curiosity Board and PC. For more details, refer to Getting Started with MCHPRT3.
- Connect the U.FL connecter on the PIC32-BZ6 to the Bluetooth®/802.15.4 tester (IQxel or others) to measure the RF power from the PIC32-BZ6.
- Check the cable loss between the PIC32-BZ6 U.FL connecter to the Bluetooth/802.15.4 tester.
- MLDO is the preferred mode of calibration. Click PMU MLDO to use the MLDO mode to perform calibration.CAUTION: OTP is limited in memory of 4k, and it can only be calibrated 10 to 15 times.
- Click Start Cal. in Cal. step 0. Condition to start the new calibration.
- Click TX P1 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P1 Tune.
- Click TX P2 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P2 Tune.
- Click TX P3 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P3 Tune.
- Click TX P4 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P4 Tune.
- Click TX P5 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P5 Tune.
- Click TX P6 Start in Cal. step 1. RF TX, enter the power level shown in the tester with the cable loss, then click TX P6 Tune.
- Click Save Cal. Data in Cal. step 2. Save data to save the calibration data into the file and the DUT.