3 Connecting the Board
To connect the board, perform the following steps:
- Connect one of the USB cables from the PC to the USB connector on the board.
- Connect LCPS to the PC with a USB cable.
- Connect LCPS to the programming header on the board.
- Connect the 5V power supply to the board.