2 Creating the Application Using MPLAB Harmony v3 and MCC
The following software and hardware tools are used for this demonstration:
- MPLAB X IDE v6.20
- MPLAB Code Configurator Plugin v5.5.1
- MPLAB XC32 Compiler v4.45
- csp v3.20.0
- PIC32CZ CA90 Curiosity Ultra Development Board
- PIC32CZ CA80 Curiosity Ultra Development Board
- SAM E70 Xplained Ultra Evaluation Kit
- SAM V71 Xplained Ultra Evaluation Kit
Note: The updated versions of the above listed tools can also be used
to create the application, and users are not restricted to use the older versions. Also,
only one of the above mentioned boards is needed for creating the application.