8.4 Configuring config.json
Configure config.json with the correct CSMS URL, port, charge point ID and security profile.
On the target, edit the file using the vi tool. For a Buildroot image, the file is located under /ocpp201/. For a Yocto Project® image, the file is located under /ocpp/.
- Set securityProfile to 0 for an unsecured test connection.
- Set ocppCsmsUrl to the URL and port displayed in the OCA interface.
- Ensure that the charge point ID in the URL matches the Unique Identifier Charging Station value in OCTT.
The WebSocket URL can be found in the OCA interface: