22.3.2.1 Register Synchronization Categories
Most of the I/O registers need to be synchronized to the asynchronous TCD core clock domain. This is done in different ways for different register categories:
- Command and Enable Control registers
- Double-buffered registers
- Static registers
- Normal I/O and STATUS registers
See Table 22-3 for categorized registers.
Command and Enable Registers
Because of synchronization between the clock domains, it is only possible to change the Enable bits while the Enable Ready bit (ENRDY) in the Status register (TCDn.STATUS) is '1'.
The Control E register commands (TCDn.CTRLE) are automatically synchronized to the TCD core domain when the TCD is enabled and as long as no synchronization is ongoing already. Check if the Command Ready bit (CCMDRDY) is '1' in TCDn.STATUS to ensure that it is possible to write a new command. TCDn.CTRLE is a strobe register that will clear itself when the command is done.
- Synchronize at the end of the TCD cycle: Synchronizes all double-buffered registers to TCD clock domain at the end of the TCD cycle.
- Synchronize: Synchronizes all double-buffered registers to the TCD clock domain when the command is synchronized to the TCD clock domain.
- Restart: Restarts the TCD counter.
- Software Capture A: Capture the TCD counter value to TCDn.CAPTUREA.
- Software Capture B: Capture the TCD counter value to TCDn.CAPTUREB.
Double-Buffered Registers
The double-buffered registers can be updated in normal I/O writes while TCD is enabled and no synchronization between the two clock domains is ongoing. Check that the CMDRDY bit in TCDn.STATUS is '1' to ensure that it is possible to update the double-buffered I/O registers. The values will be synchronized to the TCD core domain when a synchronization command is sent or when TCD is enabled.
Static Registers
The static registers are kept static whenever TCD is enabled. This means that these registers must be configured before enabling TCD. It is not possible to write to these registers as long as TCD is enabled. To see if TCD is enabled, check if ENABLE in TCDn.CTRLA is reading '1'.
Normal I/O and Status Registers
The read-only registers inform about synchronization status and values synchronized from the core domain. The reset of these registers and normal I/O registers are not constrained by any synchronization between the domains.
Enable and Command Registers | Double-Buffered Registers | Static Registers | Read-Only Registers | Normal I/O Registers |
---|---|---|---|---|
CTRLA (ENABLE bit) | TCDn.DLYCTRL | TCDn.CTRLA (All bits Except ENABLE bit) | TCDn.STATUS | TCDn.INTCTRL |
CTRLE | TCDn.DLYVAL | TCDn.CTRLB | TCDn.CAPTUREA | TCDn.INTFLAGS |
TCDn.DITCTRL | TCDn.CTRLC | TCDn.CAPTUREB | ||
TCDn.DITVAL | TCDn.CTRLD | |||
TCDn.DBGCTRL | TCDn.EVCTRLA | |||
TCDn.CMPASET | TCDn.EVCTRLB | |||
TCDn.CMPACLR | TCDn.INPUTCTRLA | |||
TCDn.CMPBSET | TCDn.INPUTCTRLB | |||
TCDn.CMPBCLR | TCDn.FAULTCTRL |