5.2.5.11 ADC Timings
The ADC start-up time is programmed using ADC_MR.STARTUP. Refer to the section “Electrical Characteristics”.
The ADC Controller provides an inherent tracking time of six ADC clock cycles.
A minimal tracking time is necessary for the ADC to ensure the best converted final value between two conversions. The tracking time can be adjusted to accommodate a range of source impedances. If more than six ADC clock cycles are required, the tracking time can be increased by using ADC_MR.TRACKTIM and ADC_EMR.TRACKX.
Warning: No input buffer amplifier
to isolate the source is included in the ADC. Refer to the section “Electrical
Characteristics”.