4.5.4.3 Reset State Priorities
The reset state manager manages the priorities among the different reset sources. The resets are listed in order of priority as follows:
- General reset
- Backup reset
- 32.768 kHz Crystal Failure Detection reset
- Main System Bus Clock (MCK0) Failure Detection reset
- Watchdog reset
- Software reset
- User reset
Specific cases are listed below:
- When in User reset:
- A watchdog event is impossible because the WDT is being reset by the Processor reset signal.
- A Software reset is impossible, since the Processor reset is being activated.
- When in Software reset:
- A watchdog event has priority over the current state.
- The NRST has no effect.
- When in Watchdog reset:
- The Processor reset is active and so a Software reset cannot be programmed.
- A User reset cannot be entered.