1.15 I2C Driver Asynchronous - I2C EEPROM

This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM.

Description

This example uses the I2C driver in asynchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an on-Board AT24MAC402 EEPROM device.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/i2c/async/i2c_eeprom/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cz_ca70_curiosity_ultra.XMPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit
pic32cz_ca70_curiosity_ultra_freertos.XMPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32cz_ca70_curiosity_ultra.X

pic32cz_ca70_curiosity_ultra_freertos.X

MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit

Setting Up PIC32CZ CA70 Curiosity Ultra Development Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and program the application using its IDE
  2. LED is turned ON when the value read from the EEPROM matched with the written value
Refer to the following table for LED name: