1.27 SPI Driver Synchronous - Multi Client

This example demonstrates how to use single instance of the SPI driver in synchronous mode to communicate with multiple EEPROMs.

Description

This example write and read data to and from two separate EEPROM connected over the same SPI bus by using the multi client feature of the driver. The example also demonstrates how to setup two different EEPROM transfers at different baud rates.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi/sync/spi_multi_slave/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cz_ca70_curiosity_ultra_freertos.XMPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription

pic32cz_ca70_curiosity_ultra_freertos.X

MPLABX project for PIC32CZ CA70 Curiosity Ultra Development Kit

Running the Application

  1. Build and program the application using its IDE
  2. The LED indicates success or failure
    • The LED turns ON when the data read from the EEPROMs matches with the data written to the EEPROMs.
Refer to the following table for LED name: