11.3.1.1.1 Physical Sections
The Flash is physically divided into two fixed sections, a Read-While-Write (RWW) section and a Non Read-While-Write (NRWW) section.
The main difference between the two sections are:
- When erasing or writing a page located inside the RWW Flash, the NRWW Flash can be read during the operation
- When erasing or writing a page located inside the NRWW Flash, the CPU is halted during the entire operation
The syntax “Read-While-Write section” refers to which section is being programmed (erased or written) and not the one read. Only the code located inside the NRWW Flash can be accessed by either executing a CPU instruction or reading data while the RWW Flash is being written or erased.
Note: Interrupt code located in the RWW section
may halt the CPU if the associated interrupt is triggered while the NRWW section is
erased or written. Either disable the interrupt or place the interrupt code in the Boot
Loader Code (BOOT) section to avoid this.
The figures and table below explain the two physical flash sections in more detail:
| Flash Section Erased/Written | Flash Section Accessed | CPU |
|---|---|---|
| NRWW section | NRWW section | Halted |
| RWW section | NRWW section | Running |
| NRWW section | RWW section | Halted |
| RWW section | RWW section | Halted |
Note: The User Row is located in the RWW Flash,
so when erasing or writing a page located in the User Row, the NRWW Flash can be read during
the operation.
Note: The physical sections sizes are
device-dependent. Refer to the Memory Overview section for details.