1.7 Observing the Output on Board and Serial Terminal
- When the application builds and completes programming, open the Tera Term tool on the PC. Select Serial Port and set the baud rate as 115200.
- Press the RESET button on the
PIC32CM LS60 Curiosity Pro Evaluation Kit, and the LED will toggle at 500 ms by
default, and with every subsequent SW0 switch press, the LED toggling rate
will change to 1s, 2s, and 4s.
Figure 1-24. LED Toggling Rate on Serial Terminal While the LED toggling rate on the Serial Terminal changes with every subsequent switch press, observe the same change in the Toggling rate of LED0 on the evaluation kit.