4 Setting Output Voltage

Figure 4-1 shows the complete feedback network needed. As the capacitors block DC voltages, the feedback resistors RFBT and RFBB will set the feedback voltage, VFB, by attenuating the buck converter output voltage, Vout. Knowing this, the Vout of the buck can be set. The resulting feedback voltage, VFB, of this voltage division will equal the internal reference voltage Vref when Vout is at the desired level. The resulting relation between the resistors and the reference voltage is given by:
This feedback controller uses the internal DAC as the reference voltage, meaning that the output voltage can be adjusted in software. It does, however, not allow for very large adjustments, as the amplifier might have undesired characteristics closer to its supply voltage.

For applications using an adjustable output regulator, the bottom resistor RFBB is replaced by a variable resistor, such as a potentiometer, as seen in Figure 4-2. This is important as the top resistor RFBT is a part of the phase compensation network in the error amplifier, while RFBB does not affect the poles of the system.