1.1.3.4.34 DRV_METROLOGY_CALIBRATION_REFS Struct
C
typedef struct {
double aimVA;
double aimIA;
double angleA;
double aimVB;
double aimIB;
double angleB;
double aimVC;
double aimIC;
double angleC;
DRV_METROLOGY_PHASE_ID lineId;
} DRV_METROLOGY_CALIBRATION_REFS;Summary
Specifies the all reference values used for the auto calibration process.
Description
Field description:
aimVA. Rms voltage applied to the voltage input (phase A). Units: Volts.
aimIA. Rms current applied to the current input (phase A). Units: Amps
angleA. Angle between the voltage and current vectors (phase A). Units: Degrees. The value is positive if the current is lagging the voltage.
aimVB. Rms voltage applied to the voltage input (phase B). Units: Volts.
aimIB. Rms current applied to the current input (phase B). Units: Amps
angleB. Angle between the voltage and current vectors (phase B). Units: Degrees. The value is positive if the current is lagging the voltage.
aimVC. Rms voltage applied to the voltage input (phase C). Units: Volts.
aimIC. Rms current applied to the current input (phase C). Units: Amps
angleC. Angle between the voltage and current vectors (phase C). Units: Degrees. The value is positive if the current is lagging the voltage.
lineId. Line identifier of the phase to calibrate.
Remarks
None.