1.2.12.4.7 SRV_QUEUE_Read_Element Function
C
SRV_QUEUE_ELEMENT *SRV_QUEUE_Read_Element(
SRV_QUEUE *queue,
uint16_t elementIndex
);Summary
Reads an element from a queue at the given index.
Description
This function reads an element from a queue at the given index.
Precondition
The queue must have been initialized previously with function SRV_QUEUE_Init.
Parameters
| Param | Description |
|---|---|
| queue | Pointer to the queue from which the element must be read |
| elementIndex | Position of the element in the queue |
Returns
Pointer to the queue element.
If the queue is empty, NULL is returned.
Example
#define NUM_MAX_NODES 750 typedef struct _node_info_tag { struct _node_info_tag *prev; struct _node_info_tag *next; uint8_t macAddress[8] } NODE_INFO; static SRV_QUEUE nodeQueue; static NODE_INFO nodeInfo1; static NODE_INFO nodeInfo2; NODE_INFO *nodeInfo3; SRV_QUEUE_Init(&nodeQueue, NUM_MAX_NODES, SRV_QUEUE_TYPE_SINGLE); memset(nodeInfo1.macAddress, 0xFF, 8); SRV_QUEUE_Append(&nodeQueue, (SRV_QUEUE_ELEMENT *)&nodeInfo1); memset(nodeInfo2.macAddress, 0xEE, 8); SRV_QUEUE_Insert_After(&nodeQueue, (SRV_QUEUE_ELEMENT *)&nodeInfo1, (SRV_QUEUE_ELEMENT *)&nodeInfo2); nodeInfo3 = SRV_QUEUE_Read_Element(&nodeQueue, 2);
Remarks
None.