1.2.12.4.6 SRV_QUEUE_Read_Or_Remove Function
C
SRV_QUEUE_ELEMENT *SRV_QUEUE_Read_Or_Remove(
SRV_QUEUE *queue,
SRV_QUEUE_MODE accessMode,
SRV_QUEUE_POSITION position
);Summary
Reads or removes an element from a queue.
Description
This function reads or removes an element from a queue.
Precondition
The queue must have been initialized previously with function SRV_QUEUE_Init.
Parameters
| Param | Description |
|---|---|
| queue | Pointer to the queue from which the element must be read or removed |
| accessMode | Access mode (read or remove) |
| position | Position in the queue to read or remove (head or tail) |
Returns
In case of remove, the element will be removed from queue and returned.
In case of read, the element will be returned without removing it from the queue.
If the queue is empty, NULL is returned.
Example
#define NUM_MAX_NODES 750 typedef struct _node_info_tag { struct _node_info_tag *prev; struct _node_info_tag *next; uint8_t macAddress[8] } NODE_INFO; static SRV_QUEUE nodeQueue; static NODE_INFO nodeInfo; NODE_INFO *removedNode; SRV_QUEUE_Init(&nodeQueue, NUM_MAX_NODES, SRV_QUEUE_TYPE_SINGLE); memset(nodeInfo.macAddress, 0xFF, 8); SRV_QUEUE_Append(&nodeQueue, (SRV_QUEUE_ELEMENT *)&nodeInfo); removedNode = SRV_QUEUE_Read_Or_Remove(&nodeQueue, SRV_QUEUE_MODE_REMOVE, SRV_QUEUE_POSITION_HEAD);
Remarks
None.