SRV_PCOUP_Get_Channel_Config Function
C
SRV_PLC_PCOUP_CHANNEL_DATA * SRV_PCOUP_Get_Channel_Config(DRV_PLC_PHY_CHANNEL channel);
Summary
Get the PLC PHY Coupling parameters for the specified PRIME channel.
Description
This function allows to get the PLC PHY Coupling parameters for the specified PRIME channel. These parameters can be sent to the PLC device through PLC Driver PIB interface (DRV_PLC_PHY_PIBSet).
Precondition
None.
Parameters
| Param | Description |
|---|---|
| channel | PRIME channel (DRV_PLC_PHY_CHANNEL Enum) for which the parameters are requested |
Returns
Pointer to SRV_PLC_PCOUP_CHANNEL_DATA Struct, containing the PLC PHY Coupling parameters
if channel parameter is valid
NULL
if channel parameter is not valid
Example
SRV_PLC_PCOUP_CHANNEL_DATA *pCoupValues; pCoupValues = SRV_PCOUP_Get_Channel_Config(SRV_PLC_PCOUP_MAIN_BRANCH);
Remarks
This function is only generated by MCC if the PLC Driver uses PRIME PHY.
If SRV_PCOUP_Set_Channel_Config function is used to set the PLC PHY Coupling parameters, this function is not needed.