2.1.10 Build and Program
The demo project will be compiled and programmed to both PIC32CXMTG-EK boards.
Build the application
- Open the project Properties by Right Clicking on the project name (pic32cxmtg)
- Make sure that XC32 compiler toolchain is selected. Press OK
Figure . Select Compiler 
- Build the application by clicking on the Build Main Project or Clean and Build Main Project menu command
Figure . Build Project 
- Verify the build is SUCCESSFUL in Output window
Figure . Successful Build 
Program the application
- Connect a micro-USB cable from computer to the USB port on the PIC32CXMTG-EK board
- Click on Make and Program Device Main Project menu command
Figure . Make And Program Device 
- If not already done, select the programming tool for the connected board
Figure . Select Programming Tool 
Repeat steps 4 and 5 for the second PIC32CXMTG-EK board