4.3 Data and Power Connection

Note: The midspan has no ON-OFF switch, simply plug the midspan into an AC power source.
Follow the procedure to connect the data and power source to the midspan unit.
  1. Connect the DATA IN (input) jack from the midspan to remote Ethernet network (item 2 in the following figure).
  2. Connect the DATA & PWR OUT (output) jack from the midspan to the terminal (item 3 in the following figure).
  3. Connect AC power lines from the LINE IN terminal (item 1 in the following figure) to main AC power. Ensure that the power outlet is nearby and easily accessible.
    Note: Connect the midspan unit to a weather-proof AC power source box that meets IP66 and IP67 ratings.
LabelDescription
1LINE INPower input, 100 VAC–240 VAC
2DATA INData in to the Ethernet (network) switch
3DATA & PWR OUTData and power out to the Ethernet terminal