2.4.3.5 FrameCheckCalculate()
static uint16_t FrameCheckCalculate (uint8_t * ftpData, uint16_t bufferLength)[static]
Calculate the frame check on the given data buffer.
Note:
For more information on the frame check used by the FTP refer to the MDFU protocol document version 1.0.0.
| in | ftpData |
Data buffer to be used for the frame check calculation |
| in | bufferLength |
Length of data objects in the buffer |
Calculated frame check |