2.1.1.5 Functions
static void CRC32_Calculate (uint32_t startAddress, uint32_t length, uint32_t *crc)
Calculates the CRC32 checksum for a specified memory region.
static bl_result_t CRC32_Validate (uint32_t startAddress, uint32_t length, uint32_t crcAddress)
Validates the CRC32 checksum for a specified memory region.
bl_result_t BL_ImageVerify (void)
Performs a verification sequence on the staging area image memory space.
bl_result_t BL_ImageVerifyById (uint8_t installLocationId)
Performs a verification sequence on the given application image memory space.
static bl_result_t BootloaderProcessorUnlock (uint8_t *bufferPtr)
Unlocks the bootloader processor using the provided buffer.
static void DownloadAreaErase (uint32_t startAddress)
Erases the entire area used to download the image data.
bl_result_t BL_Initialize (void)
Performs the initialization steps required to configure the bootloader peripherals.
bl_result_t BL_BootCommandProcess (uint8_t *commandBuffer, uint16_t commandLength)
Executes the required action based on the block type received in the bootloader data buffer.
void BL_ApplicationStart (void)
Performs actions to jump the MCU program counter to the application start address.
bool BL_CheckForcedEntry (void)
Checks the software entry flags for a forced entry into Bootloader mode.
bl_result_t BL_CopyImageAreas (uint8_t srcImageId, uint8_t destImageId)
Performs a direct internal memory copy of one image space to another.