This protocol consists of the serialization of the PRIME API primitives. The Microchip
PRIME Stack can provide the Application Programming Interface (PRIME API) through a
serial interface as an independent protocol of USI. It is available only when the user
application contains the modem example.Figure 1-7. PRIME API USI Frame
Format
The following three fields are available within the general MESSAGE DATA field:
LENGTH Extended (1 bit): As the
information contained in the message data can exceed the size reserved for MSG
length (10 bits), a bit has been added to increase the message length size. In
this field the most significant bit of the message length is codified.
PRIME API COMMAND (7 bits): This
field refers to the primitive included in the message, using the same primitives
described in the PRIME API interface description. The values for those
primitives are defined in enumerator prime_api_cmd_t in the
modem.h file.
Primitive function parameters:
The serialization of each primitive directly concatenates the different
parameters included in the primitive function, with the most significant byte of
a variable always on the left. The only exception is that the length of buffers
is always placed before the buffer itself so that the data can be inserted and
extracted easily. This is applicable to all primitives in the PRIME API.
Figure 1-8
shows how a serialized primitive looks. It is based on the
MAC_ESTABLISH.request, which is mapped into the
following type:
Figure 1-8. Message Data for
MAC_ESTABLISH.request Primitive
Important: The Base Management
primitives already include the PRIME API command as the first function
parameter, therefore exceptionally sending it twice is not
required.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.