1.2 FAT File System Using NVM Media
This application shows an example of implementing a FAT disk in the device internal Flash memory.
Description
File System Operations on NVM:
- Application places a FAT disk image consisting of a Master Boot Record (MBR) sector, Logical Boot sector, File allocation table, and Root directory area in the internal Flash memory (NVM)
- During execution, the
application first opens an existing file named
FILE.TXT
and performs following file system related operations:- SYS_FS_FileStat
- SYS_FS_FileSize
- SYS_FS_FileSeek
- SYS_FS_FileEOF
- It tries to read the file and checks if string “Data” is present. If present it continues to next step or it fails the application
- Finally, the string “Hello World” is written to this file. The string is then read and compared with the string that was written to the file. If the string compare is successful, an LED indication is provided
File System Layer Uses:
- Memory driver to communicate with underlying NVM media
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/fs/nvm_fat.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32wm_bw1_curiosity.X | MPLAB X project for PIC32WM-BW1 Curiosity board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32wm_bw1_curiosity.X | PIC32WM-BW1 Curiosity board |
Setting Up PIC32WM-BW1 Curiosity Board
- Connect the USB port on the board to the computer using a USB Type-C cable
Running the Application
- Build and program the application using its IDE.
- Press Switch to start the file operations.
- The LED is turned ON when the
FILE.TXT
file has the app data “Hello World” written in it
Refer to the following table for the Switch and LED names:
Board | Switch Name | LED Name |
---|---|---|
PIC32WM-BW1 Curiosity board | SW2 | Green LED |