1.7 Time System Service Multi-client
This example application demonstrates the multi-client system timer functionality.
Description
- This application demonstrates timer functionality (with two clients to the Time System Service) by periodically printing a message on console every two seconds and blinking an LED every one second
- Delay, counter and single shot timer functionality is demonstrated on a switch press
- On a switch press, the application reads the current value of the 64 bit counter (say, count 1)
- It then starts a delay of 500 milliseconds and waits for the delay to expire
- Once the delay has expired, the application again reads the current value of the 64 bit counter (say, count 2) and calculates the difference between the two counter values
- The difference count indicates
the time spent for the delay and is printed on the console as,
Delay time = x ms
, where x is the delay value and is equal to 500 milliseconds in the given example - The application then starts a single shot timer of 100 milliseconds
- When the single shot timer
expires, a message is printed on the console as,
Single shot timer of 100 ms expired
- This message is printed only once on every switch press
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/system/time/sys_time_multiclient.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32wm_bw1_curiosity.X | MPLAB X project for PIC32WM-BW1 Curiosity board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32wm_bw1_curiosity.X | PIC32WM-BW1 Curiosity board |
Setting Up PIC32WM-BW1 Curiosity Board
- Connect the USB port on the board to the computer using a USB Type-C cable
Running the Application
- Open the Terminal application (E.g., Tera term) on the computer.
- Connect to the USB COM port and
configure the serial settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- Build and program the application using its IDE.
- Observe the following message
getting printed on the console every two seconds.
- Press the switch and observe the
following output on the terminal (highlighted in red box).
Delay time = 500 ms
indicates the amount of time spent during the delaySingle shot timer of 100 ms expired
is printed only once on every switch press
- LED indicates the periodic timer
functionality.
- LED is toggled periodically every one second
Refer to the following table for Switch and LED names:
Board | Switch Name | LED Name |
---|---|---|
PIC32WM-BW1 Curiosity board | SW2 | Green LED |