1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32WM-BW1 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
Name | Description |
---|---|
Console Debug System Service Using UART | This example application demonstrates the Universal Asynchronous Receiver/Transmitter (UART) based console and debug system service |
FAT File System Using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
FAT File System Using SD Card Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the Serial Peripheral Interface (SPI) Peripheral Library (PLIB) |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
SPI Driver Asynchronous - Self Loopback Multi-client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the Universal Synchronous/Asynchronous Receiver/Transmitter (USART) driver in asynchronous mode |
USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |