6.2 Fuse masking
The ATtiny416 RSTPINCFG fuse is masked in the mEDBG firmware. The user is not allowed to disable UPDI (use pin as GPIO or RESET), as it will lock the debugger out of the device.
The ATtiny416 RSTPINCFG fuse is masked in the mEDBG firmware. The user is not allowed to disable UPDI (use pin as GPIO or RESET), as it will lock the debugger out of the device.