4.1 ADC Clock
Before using the ADC controller, its GCLK must be enabled in the Power Management Controller (PMC). To reach the maximum sampling rate (1 MS/s), the ADCCLK frequency, derived from the GCLK, must be 20 MHz:
fADCCLK can be set to a value lower than 20 MHz if required by the application (for example, if one of the channels used in the application needs a very long tracking time).