3.2 MCC Melody Implementation
- Create a new MPLAB X IDE project for AVR16EB32.
- Open MCC from the toolbar (more information on installing the MCC plug-in can be found here).
- In MCC Content Manager Wizard, select MCC Melody, then click Finish.
- From the Device
Resources, go to Drivers window, Timer and add TCE module,
then do the following configuration:
– Module Enable - toggle the button (it turns blue if enabled).
- From the Device Resources,
go to Drivers window, add the WEX module, then do the following
configuration:
– Input Matrix: Direct
– Update Source: TCE (the update condition for the output signals will be the TCE module)
– Override Settings: Check all the boxes from the Output Enable column for the Waveform Output[0-7]
– Pattern Generation Mode Enable: Toggle the button (it turns blue if enabled)
– Pattern Generation Actions: Check all the boxes from the Override Enable column and set for each output a desired state (LOW or HIGH), to set a pattern
- In the Pin Grid View window - check if the WEX_WO[0-7] pins are locked as outputs on PORTA. The pins are locked when the boxes from Output Enable column from Override Settings are checked. To change the PORT,click on a pin from another PORT in Pin Grid View.
- In the Project Resources window, click the Generate button so that MCC will generate all the specified drivers and configurations.
- Edit the main.c file, as
following:
Add in the include files section:
#include "mcc_generated_files/system/system.h" #include <util/delay.h>Add macro definitions:
/* Patterns that are written in the PGMOUT register */ #define COMPLEMENTARY_PATTERN (WEX_PGMOUT6_bm | WEX_PGMOUT4_bm | WEX_PGMOUT2_bm | WEX_PGMOUT0_bm) #define STAIRCASE0_PATTERN (WEX_PGMOUT0_bm) #define STAIRCASE1_PATTERN (WEX_PGMOUT1_bm) #define STAIRCASE2_PATTERN (WEX_PGMOUT2_bm) #define STAIRCASE3_PATTERN (WEX_PGMOUT3_bm) #define STAIRCASE4_PATTERN (WEX_PGMOUT4_bm) #define STAIRCASE5_PATTERN (WEX_PGMOUT5_bm) #define STAIRCASE6_PATTERN (WEX_PGMOUT6_bm) #define STAIRCASE7_PATTERN (WEX_PGMOUT7_bm) #define PATTERN_RESET (0x00)Add functions:
void Complementary_Pattern_Set(void) { WEX0_PatternGenerationOutputSet(COMPLEMENTARY_PATTERN); uint8_t complementary_pattern = COMPLEMENTARY_PATTERN; _delay_us(25); /* Complementary signals pattern */ for(uint8_t i = 0; i < 9; i++) { /* Complementary_pattern variable changes at every step */ complementary_pattern = ~complementary_pattern; /* Toggle the pattern for each of the WEX's output */ WEX0_PatternGenerationOutputSet(complementary_pattern); /* Software delay added in order for the toggle to be visible */ _delay_us(25); } /* Put all signals in low '0' logic and wait 250us to see the transition from one of * the complementary patterns to the stairs pattern*/ WEX0_PatternGenerationOutputSet(PATTERN_RESET); } void Stairs_Pattern_Set(void) { /* Each of the signals switch from low to high one at a time in increasing order * generate a stairs increment pattern*/ WEX0_PatternGenerationOutputSet(STAIRCASE7_PATTERN); /* Software delay added in order for the increment to be visible */ _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE6_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE5_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE4_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE3_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE2_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE1_PATTERN); _delay_us(5); /* Each of the signals switch from low to high one at a time in decreasing order * generate a stairs decrement pattern*/ WEX0_PatternGenerationOutputSet(STAIRCASE0_PATTERN); /* Software delay added in order for the decrement to be visible */ _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE1_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE2_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE3_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE4_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE5_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE6_PATTERN); _delay_us(5); WEX0_PatternGenerationOutputSet(STAIRCASE7_PATTERN); _delay_us(5); /* Put all signals in low '0' logic and wait 250us to see the transition from the * stairs pattern to one of the complementary patterns */ WEX0_PatternGenerationOutputSet(PATTERN_RESET); }Edit the main function:
int main(void) { SYSTEM_Initialize(); while(1) { Complementary_Pattern_Set(); _delay_us(250); Stairs_Pattern_Set(); _delay_us(250); } }
- Now, the project can be built and run using MPLAB X IDE.