35.3.1 Initialization
To initialize the OPAMP peripheral for basic, always-on operation, the following
steps are recommended:
- Configure the timebase of the OPAMP peripheral by writing to the Timebase (TIMEBASE) bit field in the Timebase (OPAMP.TIMEBASE) register.
- For each op amp that will be used:
- Configure the Op Amp n Input Multiplexer (OPAMP.OPnINMUX):
- Select the non-inverting (+) input of the op amp by writing to the Multiplexer for Positive Input (MUXPOS) bit field
- Select the inverting (-) input of the op amp by writing to the Multiplexer for Negative Input (MUXNEG) bit field
- Configure the Op Amp n Resistor Ladder Multiplexer (OPAMP.OPnRESMUX):
- Select the connection to the top resistor in the resistor ladder by writing to the Multiplexer for Top (MUXTOP) bit field
- Select the connection to the bottom resistor in the resistor ladder by writing to the Multiplexer for Bottom (MUXBOT) bit field
- Select the wiper position in the resistor ladder by writing to the Multiplexer for Wiper (MUXWIP) bit field
- Configure the Op Amp n Control A (OPAMP.OPnCTRLA) register:
- Configure the op amp to be always
on by writing ‘
1’ to the Always On (ALWAYSON) bit - Disable events for the op amp by
writing ‘
0’ to the Event Enable (EVENTEN) bit - Select the normal output mode by writing the NORMAL setting to the Output Mode (OUTMODE) bit field
- Configure the op amp to be always
on by writing ‘
- Optional: Configure the allowed settling time by writing to the Settle Timer (SETTLE) bit field in the Op Amp n Settle Timer (OPAMP.OPnSETTLE) register.
- Configure the Op Amp n Input Multiplexer (OPAMP.OPnINMUX):
- Enable the OPAMP peripheral by writing a
‘
1’ to the OPAMP Enable (ENABLE) bit in the Control A (OPAMP.CTRLA) register. - For each op amp whose settling time was
configured in step 2.4 above, wait for the SETTLED bit in the Op Amp n Status
(OPAMP.OPnSTATUS) register to become ‘
1’. This indicates that the op amp start-up and settling have completed, and the OPAMP peripheral is ready for use.