4.3.3 Calibration Flow Demonstration

In this demonstration, the user can calibrate TX parameters and RX parameters of the PIC32CX-BZ2 using a PC with the installed MCHPRT3 tool.

Perform the following steps for the demonstration of the calibration flow (see the following figure):

  1. Set up the connection between the PIC32 WBZ451 Curiosity Board and PC. For more details, refer to Getting Started with MCHPRT3.
  2. Connect the U.FL connecter on the PIC32CX-BZ2 to Bluetooth/Zigbee tester (IQxel or others) to measure the RF power from the PIC32CX-BZ2.
  3. Check the cable loss between the PIC32CX-BZ2 U.FL connecter to the Bluetooth/Zigbee tester.
  4. MLDO is the preferred mode of calibration. Click PMU MLDO to use the MLDO mode to perform calibration.
  5. Enter Cable loss, and select Save IB type (Flash/OTP) and DUT Mode (MPA+LPA/LPA only).
    CAUTION: OTP is limited in memory of 4k, and it can only be calibrated for 10 to 15 times.
  6. Click Start Cal. to start the new calibration.
  7. Click Freq. Start in Cal. step 1. Freq., the DUT transmits the Bluetooth Low Energy packet at 2440 MHz.
  8. Check the carrier frequency at the tester and click Freq. decrease or Freq. increase to change the carrier frequency.
  9. Once the carrier frequency is close to 2440 MHz, click Freq. Done.
  10. Click MPA Start in Cal. step 2. RF Power; read the power level in the tester, then enter it in the tool.
  11. Click MPA Power Tune in Cal. step 2. RF Power; repeat steps 10 and 11 until the power level reaches the target power, 8 dBm ±0.5 dB.
  12. Click LPA Start in Cal. step 2. RF Power; read the power level in the tester, then enter it in the tool.
  13. Click LPA Power Tune in Cal. step 2. RF Power; repeat steps 12 and 13 until the power level reaches the target power, 4 dBm ±0.5 dB.
  14. If it is LPA only in the DUT Mode, the LPA target power would be 5.5 dBm ±0.5 dB.
  15. Click LOFT/TXIQ/FLT Calibration in Cal. step 3. LOFT/TXIQ/FLT, then wait for done.
  16. Click Save Cal. Data in Cal. step 4. Save data to save the calibration data into the file and the DUT.
Figure 4-15. MCHPRT3 PIC32CX-BZ2 GUI for Calibration Flow Demonstration
Figure 4-16. Calibration Setup