3.5.3 -p,
--processor=PROC
Specify the target processor, e.g.:
xc32-as -p32AK1216GC41064 file.s
The assembler defines macros based on the target processor setting, which
can be tested by conditional directives in source code. For example, include file
p32AK1216GC41064.inc contains
the following:
.ifndef __32AK1216GC41064
.error “Include file does not match processor setting”
.endif
In addition to the target processor, a macro to identify the device family is also defined. For example:
.ifdef __PIC32A
.print “PIC32A family selected”
.endif
Macros for the device families (see Predefined Symbols) are defined based on target processor setting.