3.2.5 --listing-cont-lines
#
The --listing-cont-lines option is used to set the
maximum number of continuation lines used for the output data column of the listing. By
default, this is 8. The following lines are extracted from a listing that was created
without using the --listing-cont-lines option. The text in bold shows
the continuation lines used for the output data column of the listing.
2 0000 54 68 69 73 .ascii "This is a long character sequence."
2 20 69 73 20
2 61 20 6C 6F
2 6E 67 20 63
2 68 61 72 61
2 63 74 65 72
2 20 73 65 71
2 75 65 6E 63
2 65 2E
Notice that the number of bytes displayed matches the number of bytes in
the ASCII string; however, if the option --listing-cont-lines 2 is
used, then the output data will be truncated after 2 continuation lines as shown
below.
2 0000 54 68 69 73 .ascii "This is a long character sequence."
2 20 69 73 20
2 61 20 6C 6F