11.3.3.7 stack
The stack attribute specifies that a section should be designated for use as the processor stack. On PIC32A MCU devices, there are no restrictions on stack allocation. The following attributes may be used in conjunction with stack and will further specify the allocation:
address()specifies an absolute addressalign()specifies alignment of the section starting address