11.3.3.4 persist [DD]
The persist attribute specifies that a section should be allocated as persistent storage in data memory, as defined by region data in the linker script. Persistent storage is not cleared or initialized by the C run-time library. The following attributes may be used in conjunction with persist and will further specify the allocation:
address()specifies an absolute addressnearspecifies the first 64K of data memoryxmemoryspecifies X address space, which includes all of region data below the address __YDATA_BASE as defined in the linker scriptymemoryspecifies Y address space, which includes all of region data above the address __YDATA_BASE as defined in the linker scriptalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1