1.1.3 PIC32CZ CA70 Curiosity Ultra Development Board: Building and Running the USB Device HID Bootloader applications
Downloading and building the application
To clone or download these application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can be download using MCC content manager by following these instructions.
Path of the application within the repository is apps/usb_device_hid_bootloader/
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
Project Name | Description |
---|---|
bootloader/firmware/pic32cz_ca70_cult.X | MPLABX Project for PIC32CZ CA70 Curiosity Ultra Development Board |
Test Application
Project Name | Description |
---|---|
test_app/firmware/pic32cz_ca70_cult.X | MPLABX Project for PIC32CZ CA70 Curiosity Ultra Development Board |
Setting up PIC32CZ CA70 Curiosity Ultra Development Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Use TARGET USB J203 connector on the board to connect the USB Device to the USB Host PC
Running the Application
Open the test application project test_app/firmware/pic32cz_ca70_cult.X in the IDE
Build the project to generate the binary (Do not program the binary)
Open the bootloader project bootloader/firmware/pic32cz_ca70_cult.X in the IDE
Build and program the application using the IDE
Once programming is completed and bootloader starts running
- LED0 will be Turned On
- HID Custom device with product ID 3C will be enumerated on Host PC
Open the Terminal application (Ex.:Tera Term) on the computer to get test application messages through UART once bootloaded
Configure the serial port settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Launch the Unified Host application from below path
- <harmony3_path>/bootloader/tools/UnifiedHost-*/UnifiedHost-*.jar
Configure the Unified host application
Select the Device architecture and Protocol as shown below
Click on configure button and select the USB Device as 3C
Load the test application hex file to be programmed using below option
- <harmony3_path>/bootloader_apps_usb/apps/usb_device_hid_bootloader/test_app/firmware/pic32cz_ca70_cult.X/dist/sam_e70_xult/production/pic32cz_ca70_cult.X.production.hex
Open the Console window of the host application to view application bootloading sequence
Click on Program Device button to program the loaded test application hex file on to the device
Following snapshot shows output of successfully programming the test application
If above step is successful then LED1 should start blinking and the user should see below output on the console
Press and hold the Switch SW0 to trigger Bootloader from test application and the user should see below output
Repeat Steps 10-12 once and jump to Step-15
- This step is to verify that bootloader is running after triggering bootloader from test application in Step 13
Press and hold the Switch SW0 and then press Reset button or Power cycle the device to force trigger bootloader at startup
Repeat Steps 10-12 once
- This step is to verify whether bootloader is triggered by switch press at reset
Additional Steps (Optional)
To bootload any other application refer to the Application Configurations
Once done repeat the applicable steps mentioned in Running The Application