1.1.14 PIC32WM BZ6 Curiosity Evaluation Board: Building and Running the USB Device HID Bootloader applications

Downloading and building the application

To clone or download these application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can be download using MCC content manager by following these instructions.

Path of the application within the repository is apps/usb_device_hid_bootloader/

To build the application, refer to the following table and open the project using its IDE.

Setting up PIC32WM BZ6 Curiosity Evaluation Board

  • Connect the Debug USB J100 port on the board to the computer using a micro USB cable
  • Use TARGET USB J103 connector on the board to connect the USB Device to the USB Host PC

Running the Application

  1. Open the test application project test_app/firmware//pic32wm_bz6_curiosity.X in the IDE

  2. Build the project to generate the binary (Do not program the binary)

  3. Open the bootloader project bootloader/firmware//pic32wm_bz6_curiosity.X in the IDE

  4. Build and program the application using the IDE

  5. Once programming is completed and bootloader starts running

    • RGB_LED (GREEN) will be Turned On
    • HID Custom device with product ID 3C will be enumerated on Host PC
  6. Open the Terminal application (Ex.:Tera Term) on the computer to get test application messages through UART once bootloaded

  7. Configure the serial port settings as follows:

    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  8. Launch the Unified Host application from below path

    • <harmony3_path>/bootloader/tools/UnifiedHost-*/UnifiedHost-*.jar
  9. Configure the Unified host application

    • Select the Device architecture and Protocol as shown below

      hostConfig
    • Click on configure button and select the USB Device as 3C

      hostUSBSetting
    • Load the test application hex file to be programmed using below option

      • <harmony3_path>/bootloader_apps_usb/apps/usb_device_hid_bootloader/test_app/firmware/pic32wm_bz6_curiosity.X/dist/pic32wm_bz6_curiosity/production//pic32wm_bz6_curiosity.X.production.hex
      hostLoadHex
    • Open the Console window of the host application to view application bootloading sequence

      hostToolsConsole
  10. Click on Program Device button to program the loaded test application hex file on to the device

    hostProgramDevice
  11. Following snapshot shows output of successfully programming the test application

    hostSuccess
  12. If above step is successful then RGB_LED (GREEN) should start blinking and the user should see below output on the console

    output
  13. Press and hold the Switch SW0 to trigger Bootloader from test application and the user should see below output

    output
  14. Repeat Steps 10-12 once and jump to Step-15

    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 13
  15. Press and hold the Switch USR BTN 1 and then press Reset button or Power cycle the device to force trigger bootloader at startup

  16. Repeat Steps 10-12 once

    • This step is to verify whether bootloader is triggered by switch press at reset