1.1.4 SAMA7D65-Curiosity Board: Building and Running the USB Bootloader With NAND Flash Media Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file.

Path of the application within the repository is apps/mpu_usb_bootloader/.

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader_nand_flash/sama7d65_curiosity.XMPLABX Project for SAMA7D65-Curiosity Board

Test Application

Project NameDescription
test_app/sama7d65_curiosity.XMPLABX Project for SAMA7D65-Curiosity Board

Setting Up SAMA7D65-Curiosity Board

  • Connect the UART DEBUG J35 on curiosity board to the computer using a UART-FTDI cable (to enable debug com port)
  • Connect the USBA port J3 on the curiosity board to the computer using a Type-C USB cable (to power the board)
  • Close jumper J36 (NAND BOOT) on the Curiosity board

Running the Application

  1. Open the test application project test_app/sama7d65_curiosity.X in the IDE.

  2. Build the project to generate the binary (Do not program the binary).

  3. Open the bootloader project usb_device_hid_bootloader/bootloader_nand_flash/sama7d65_curiosity.X in the IDE.

  4. Build the project to generate the harmony_bootloader.bin binary (Do not program the binary).

  5. Download and unzip SAM-BA.

  6. Open the command prompt and change the current directory to <harmony3_path>/bootloader_apps_usb/deps/at91bootstrap_binaries_sam_a7d65_curiosity/nand_flash/ and run the below command:

     <sam-ba_path>/sam-ba.exe -p usb -b sama7d65-curiosity -a nandflash -c erase::0x40000 -c write:boot.bin
  7. Change the current directory to <harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/usb_device_hid_bootloader/bootloader_nand_flash/sama7d65_curiosity.X/dist/sama7d65_curiosity/production/ and run the below command:

     <sam-ba_path>/sam-ba.exe -p usb -b sama7d65-curiosity -a nandflash -c erase:0x40000:0x80000 -c write:harmony_bootloader.bin:0x40000
  8. Reset or Power cycle the device. Green LED will be turned-on to indicate that harmony bootloader code is running on the target.

  9. Once programming is completed and bootloader starts running.

    • HID Custom device with product ID 3C will be enumerated on Host PC
  10. Open the Terminal application (Ex.:Tera Term) on the computer to get test application messages through UART once bootloaded.

  11. Configure the serial port settings as follows:

    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  12. Launch the Unified Host application from below path:

    • <harmony3_path>/bootloader/tools/UnifiedHost-*/UnifiedHost-*.jar
  13. Configure the Unified host application.

    • Select the Device architecture and Protocol as shown below

      hostConfig
    • Click the Configure button and select the USB Device as 3C

      hostUSBSetting
    • Load the test application hex file to be programmed using below option

      • <harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/test_app/sama7d65_curiosity.X/dist/sama7d65_curiosity/production/sama7d65_curiosity.X.production.hex
      hostLoadHex
    • Open the Console window of the host application to view application bootloading sequence

      hostToolsConsole
  14. Click the Program Device button to program the loaded test application hex file on to the device.

    hostProgramDevice
  15. Following figure shows output of successfully programming the test application.

    hostSuccess
  16. If above step is successful then Green LED should start blinking and the user should see below output on the console.

    output
  17. Press and hold the Switch USER and then press Reset button or Power cycle the device to force trigger bootloader at startup.

  18. Repeat Steps 14-16 once.

    • This step is to verify whether bootloader is triggered by switch press at reset