1.3.3 PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto): Building and Running the USB Live Update applications
Downloading and building the application
To clone or download these application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can be download using content manager by following these instructions.
Path of the application within the repository is apps/usb_live_update/
To build the application, refer to the following table and open the project using its IDE.
Switcher Application
| Project Name | Description |
|---|---|
| switcher/firmware/pic32mz_das_sk.X | MPLABX Project for PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto) |
Live Update Application
| Project Name | Description |
|---|---|
| live_update_app/firmware/pic32mz_das_sk.X | MPLABX Project for PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto) |
Setting up PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto)
Connect a micro USB cable to the UART-USB port J5
For programming, connect a micro USB cable to the USB Debug port J19
Use the micro-A/B port J6 (which is located on the bottom side of the board) to connect the USB Device to the USB Host PC
Running the Application
Open the switcher application project switcher/firmware/pic32mz_das_sk.X in the IDE
Make sure that the live_update_app/firmware/pic32mz_das_sk.X is added as a loadable project to switcher application
- As the Switcher application does not have any programming capabilities, Adding the live_update_app as loadable allows MPLAB X to create a unified hex file and program both these application in thier respective memory location based on the respective linker scripts

Open the Terminal application (Ex.:Tera Term) on the computer to get live update application messages through UART once loaded
Configure the serial port settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and program the switcher application using the IDE
LED3 should start blinking once programming is completed and below message has to be displayed on the Console
- The user can see how the live update application was loaded in BANK 1 by IDE and switcher application jumped BANK 1 to run it
- HID Custom device with product ID 3C will be enumerated on Host PC

Launch the Unified Host application from below path
- <harmony3_path>/bootloader/tools/UnifiedHost-*/UnifiedHost-*.jar
Configure the Unified host application
Select the Device architecture and Protocol as shown below

Click on configure button and select the USB Device as 3C

Load the live update application hex file to be programmed using below option
- <harmony3_path>/bootloader_apps_usb/apps/usb_live_update/live_update_app/firmware/pic32mz_das_sk.X/dist/pic32mz_das_sk/production/pic32mz_das_sk.X.production.hex

Open the Console window of the host application to view application bootloading sequence

Click on Program Device button to program the loaded live update application hex file on to the device
- The user can note that throughout the programming sequence and after programming the LED3 will be blinking as the application task is running along with bootloader task (Live Update Feature)

Following snapshot shows output of successfully programming the test application
- Ignore the Device Reset Messages from the host tool. The live update application ignores the reset command received and waits for a switch press to update serial number and reset

Press the Switch SW1 to update serial of Inactive Bank and trigger reset. The user should see below output on success
- This step shows that the new firmware programmed in BANK 2 is running which is mapped to lower region by switcher at reset

Repeat Steps 9-11 for further updates and observe the Banks from which application is running at every update
Configurations to be Noted
Switcher Application
- As the users are using custom linker script for Switcher, the default linker file generation has to be disabled.

Live Update Application
- Enable Live Update Option to configure USB Device HID bootloader in Live Update Mode.

- Normalize hex file:
- Check the Normalize hex file option as shown below, as the Unified bootloader host application takes hex file as an input. Normalizing the hex file will make sure the data in the hex file is arranged sequentially.