1.1.6 SAMA7D65 Curiosity Board: Building and Running the USB Device HID Bootloader With Serial Flash Media Applications
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file.
Path of the application within the repository is apps/mpu_usb_bootloader/.
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader_serial_flash/sama7d65/sam_a7d65_curiosity.X | MPLAB X Project for SAMA7D65 Curiosity Board |
Test Application
| Project Name | Description |
|---|---|
| test_app/sama7d65/sam_a7d65_curiosity.X | MPLAB X Project for SAMA7D65 Curiosity Board |
Setting Up SAMA7D65 Curiosity Board
- Connect the UART Debug port (J35) on the Curiosity board to the computer using a FTDI-USB cable (to enable Debug COM port)
- Connect the USBA port J3 on the Curiosity board to the computer using a USB Type-C cable (to power the board)
- Close jumper J39 (QSPI BOOT) on the Curiosity board
Running the Application
- Open the test application project test_app/sam_a7d65_curiosity.X in the IDE.
- Build the project to generate the binary (Do not program the binary).
- Open the bootloader project usb_device_hid_bootloader/bootloader_serial_flash/sam_a7d65_curiosity.X in the IDE.
- Build the project to generate the harmony_bootloader.bin binary (Do not program the binary).
- Download and unzip SAM-BA.
- Open the command prompt and change the current directory to
<harmony3_path>/bootloader_apps_usb/deps/at91bootstrap_binaries_sam_a7d65_curiosity/qspi_flash/
and run the below
command:
<sam-ba_path>/sam-ba.exe -p usb -b sama7d65-curiosity -t 5 -a qspiflash -c erase::0x40000 -c write:boot.bin
- Change the current directory to
<harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/usb_device_hid_bootloader/bootloader_serial_flash/sama7d65_curiosity.X/dist/sama7d65_curiosity/production/
and run the below
command:
<sam-ba_path>/sam-ba.exe -p usb -b sama7d65-curiosity -t 5 -a qspiflash -c erase:0x40000:0xa0000 -c write:harmony_bootloader.bin:0x40000
- Reset or Power cycle the device. Green LED will be turned-on to indicate that harmony bootloader code is running on the target.
- Once programming is completed and bootloader starts running.
- HID Custom device with product ID 3C will be enumerated on Host PC
- Open the Terminal application (e.g., Tera Term) on the computer to get test application messages through UART once bootloaded.
- Configure the serial port settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- Launch the Unified Host application from below path:
- <harmony3_path>/bootloader/tools/UnifiedHost-*/UnifiedHost-*.jar
- Configure the Unified host application:
- Select the Device Architecture and Protocol as shown below

- Click the Configure button and select the USB Device as
3C

- Load the test application hex file to be programmed using below
option
- <harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/test_app/sam_a7d65_curiosity.X/dist/sam_a7d65_curiosity/production/sam_a7d65_curiosity.X.production.hex

- Open the Console window of the host application to view application
bootloading sequence

- Select the Device Architecture and Protocol as shown below
- Click the Program Device button to program the loaded test application
hex file on to the device.

- Following figure shows output of successfully programming the test
application.

- If above step is successful then Green LED should start blinking and the user
should see below output on the console.

- Press and hold the Switch USER and then press Reset button or Power cycle the device to force trigger bootloader at startup.
- Repeat Steps 14-16 once.
- This step is to verify whether bootloader is triggered by switch press at reset
Additional Steps (Optional)
- To bootload any other application, refer to the Application Configurations
- Once done, repeat the applicable steps mentioned in Running the Application