1.1.2 SAM9X75 Curiosity Board: Building and Running the USB Device HID Bootloader With SD/eMMC Media Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file.

Path of the application within the repository is apps/mpu_usb_bootloader/.

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader_sd_emmc/sam9x75/sam_9x75_curiosity.XMPLAB X Project for SAM9X75 Curiosity Board

Test Application

Project NameDescription
test_app/sam9x75/sam_9x75_curiosity.XMPLAB X Project for SAM9X75 Curiosity Board

Setting Up SAM9X75 Curiosity Board

  • Connect the UART DEBUG J35 on Curiosity board to the computer using a UART-FTDI cable (to enable Debug COM port)
  • Connect the USB port J2 on Curiosity board to the computer using a micro USB cable (to power the board)
  • SD card with FAT32 file system on the Curiosity board

Running the Application

  1. Open the Terminal application (e.g., Tera Term) on the computer.
  2. Configure the serial port settings as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  3. Open the bootloader project bootloader_sd_emmc/sam9x75/sam_9x75_curiosity.X in the IDE.
  4. Build the project to generate the harmony_bootloader.bin binary (Do not program the binary).
  5. Copy the MPU bootstrap loader binary (boot.bin) from <harmony3_path>/bootloader_apps_usb/deps/at91bootstrap_binaries_sam_9x75_curiosity/bootloader/sd_card/boot.bin onto the SD card.
  6. Copy the harmony bootloader binary (harmony_bootloader.bin) from <harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/usb_device_hid_bootloader/bootloader_sd_emmc/sam_9x75_curiosity.X/dist/sam_9x75_curiosity/production/harmony_bootloader.bin onto the SD card.
  7. Insert the SD card into SD BOOT connector J14 on the target board.
  8. Reset or Power cycle the device. Green LED will be turned-on to indicate that harmony bootloader code is running on the target.
  9. Configure the Unified host application:
    • Select the Device Architecture and Protocol as shown below
    • Click the Configure button and select the USB Device as 3C
    • Load the test application hex file to be programmed using below option
      • <harmony3_path>/bootloader_apps_usb/apps/mpu_usb_bootloader/test_app/sam_9x75_curiosity.X/dist/sam_9x75_curiosity/production/sam_9x75_curiosity.X.production.hex
    • Open the Console window of the host application to view application bootloading sequence
  10. Click the Program Device button to program the loaded test application hex file on to the device.
  11. Following figure shows output of successfully programming the test application.
  12. If above step is successful then Green LED should start blinking and the user should see below output on the console.
  13. Press and hold the Switch USER and then press Reset button or Power cycle the device to force trigger bootloader at startup.
  14. Repeat Steps 10-12 once.
    • This step is to verify whether bootloader is triggered by switch press at reset