9.6.7.7 Loadaddr Built-in Function
The LOADADDR(section) built-in function
returns the absolute LMA of the named section. This is normally returns the same address as
ADDR, but it may be different if the
AT attribute is used in the output section definition (see Sections Command).