9.5.5.9.4 Output Section Fill
A fill pattern can be set for an entire section by using
=fillexp. The
fillexp is an expression. Any otherwise unspecified
regions of memory within the output section (for example, gaps left due to the required
alignment of input sections) will be filled with the two least significant bytes of the
value, repeated as necessary.
The fill value can also be changed with a FILL command in the output section commands; see Output Section Data.
Here is a simple
example:
SECTIONS { .text : { * (.text) } =0x9090 }