3.6.2 I: Specify Assembler Search Path Option
The -I dir option adds
dir to the list of directories that the assembler
searches for files specified in .include directives. You
may use -I as many times as necessary to include a number
of paths. The current working directory is always searched first; after that, the assembler
searches any -I directories in the same order as they
were specified (left to right) on the command line.
When passed directly to the assembler, this option affects the search path
used by the assembler's .include directive. To affect the
search path used by the C preprocessor for a #include
directive, pass the corresponding option to the xc32-gcc compilation
driver.