6.4.2 NVM Unlock Sequence
The unlock sequence is a mechanism that protects the NVM from unintended self-write
programming or erasing. The sequence must be executed and completed without interruption
to successfully complete any of the following operations:
- Program Flash Memory Row Erase
- Load of Program Flash Memory write latches
- Write of Program Flash Memory write latches to program memory
- Write of Program Flash Memory write latches to User IDs
- Write to EEPROM
The unlock sequence consists of the following steps and must be completed in order:
- Write
0x55to NVMCON2 - Write
0xAAto NMVCON2 - Set the WR bit of NVMCON1
Once the WR bit is set, the processor will stall internal operations until the operation
is complete and then resume with the next instruction.
Important: The two
NOP
instructions after setting the WR bit, that were required in previous devices, are
not required for PIC16(L)F184XX devices. See Figure 6-2 for an example of the unlock
sequence.Since the unlock sequence must not be interrupted, global interrupts must be disabled prior to the unlock sequence and re-enabled after the unlock sequence is completed.
NVM Unlock Sequence
BCF INTCON, GIE ; Recommended to prevent interruptions BANKSEL NVMCON1 ; BSF NVMCON1, WREN ; Enable write/erase MOVLW 55h ; Load 55h MOVWF NVMCON2 ; Step 1: Load 55h into NVMCON2 MOVLW AAh ; Step 2: Load W with AAh MOVWF NVMCON2 ; Step 3: Load AAH into NVMCON2 BSF NVMCON1, WR ; Step 4: Set WR bit to begin write/erase BSF INTCON, GIE ; Re-enable interrupts
Note:
- Sequence begins when NVMCON2 is written; steps 1-4 must occur in the cycle-accurate order shown.
- Opcodes shown are illustrative; any instruction that has the indicated effect may be used.