3.7.1 Smart Lock Application on PIC32CM LS60 Smart Lock Reference Board

Download

Description

The application showcases key-less secure access control and monitoring of a deadbolt through multiple methods:

  • Capacitive Touch keypad
    • Multiple unique user passkeys
  • Smartphone App
    • Secure bluetooth control
    • Remote access control using WiFi with AWS cloud

Modules/Technology Used

  • Peripheral Modules
    • ADC
    • EIC
    • EVSYS
    • NVMCTRL
    • PTC
    • RTC
    • SERCOM (SPI)
    • SERCOM (USART)
    • SERCOM (I2C)
    • TC
  • Drivers
    • ATECC608
  • System service
    • TIME
  • Tools
    • Secure STDIO
  • Libraries
    • Touch Library
    • Crypto Authentication Library

Hardware Used

  1. PIC32CM LS60 Smart Lock Reference Board - 1 .
  2. WFI32-IoT Development Board: EV36W50A - 2 .
  3. BM70 Compact Demo Board: BM-70-CDB - 2.
  4. Power and Motor Control Board - 1.
  5. Four AA 1.5V alkaline batteries - 2.
  6. QT3 XPLAINED PRO EXTENSION KIT: ATQT3-XPRO - 1.
  7. Schlage Deadbolt with motor and custom printed interface for limit switch - 1.
Note:
  1. Contact Microchip technical support or local Microchip FAE for purchasing the Smart Door Lock kit bundle.
  2. Not provided as part of the Smart Door Lock kit bundle. Should be procured separately (through Microchip Direct or any thirdparty vendor).

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/default.

  • Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
  • Any Serial Terminal application like Tera Term terminal application.

Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Setup

The demo can be run in three different modes:

  1. Standalone Touch keypad entry.
  2. Bluetooth control using BM70 Compact Demo Board and Smartphone application.
  3. WiFi control using WFI32-IoT Development Board and AWS cloud.

Standalone Touch Keypad Entry

Connect the QT3 Xplained pro, Power board and the deadbolt to the PIC32CM LS60 Smart Lock Reference Board as seen below:

On powering the kit, the Smart Door Lock becomes functional and waits for the user input through the Touch Keypad to control the entry access. This kit allows up to five user-authenticated entries through the door lock, and each user has a user ID (1, 2, 3 , 4 and 5). Each user would require a passkey to enter through the Touch Keypad to open the lock.

User Entry/Passkey Authentication
  1. Select a user ID (press any number from 2 to 5)1 and press "#".
  2. Enter the 5-digit passkey2 corresponding to the selected user and then press "#".
  3. If the passkey is valid, the door opens.
  4. The door automatically relocks after 10 seconds.
Note:
  1. User ID 1 is for the temporary passkey generated using the Mobile app. This user ID cannot be used without provisioning the mobile app.
  2. By default, all users (2, 3, 4 and 5) have the same passkey - '12345'.
Passkey Modification

The passkey of each user can be altered through the touch keypad using the steps outlined below.

  1. Long press “#” button until all the touch LEDs blink in the Touch Keypad.
  2. Enter the corresponding user ID which needs to be changed and press “#” 1.
  3. Enter the current passkey, and press ‘#’ to authenticate the user2.
  4. Once authenticated, enter the new passkey and press “#”.
  5. To reconfirm, enter the new passkey again and press “#”.
  6. This configures the lock with the new Passkey.
Note:
  1. User ID 1 is for the temporary passkey generated using the Mobile app.
  2. If this is the first-time configuration, enter the default passkey (12345) for validation and press “#”
  • Activate the touchpad using the palm.
  • Only 5-digit passcodes can be stored, but any number of digits can be entered on the touch keypad; only the final 5 before pressing '#' will be accepted.

Bluetooth and WiFi Control using Smartphone

A custom Android application must be installed in the smartphone to control the door lock module. Click here to download the .apk file for the app. After installing the app, it needs to be provisioned so that the mobile and the door lock device can be securely connected. Create a. Create a Microchip Technical Support case for provisioning the smartphone with the bluetooth module.

Add the following details to the support case:

Case Reason: Hardware/Firmware SupportSubject: Smart Door Lock: Primary provisioning token requestPrimary Target Device: PIC32CM5164LS60064Case Description: < share BLE MAC ID of the BM70 board >.

Programming hex file

Connect Atmel ICE or PICKIT4 or any other programmer that supports SWD programming to the J1 header on the PIC32CM LS60 Smart Lock Reference Board.

The pre-built hex file can then be programmed by following the below steps:

Steps to program the hex file
  • Open MPLAB X IDE.
  • Close all existing projects in IDE, if any project is opened.
  • Go to File -> Import -> Hex/ELF File.
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file.
      • Select Device as PIC32CM5164LS60064.
      • Ensure the proper tool is selected under Hardware Tool and click on Next button.
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click on Finish button
  • In MPLAB X IDE, click on Make and Program Device button to program the device.
  • Follow the steps in Running the Demo section below.

Programming/Debugging Application Project

  • Open the project (pic32cm_ls60_rd_smart_lock/firmware/pic32cm_ls60_rd_smart_lock/pic32cm_ls60_sdlgroup) in MPLAB X IDE.
  • Ensure proper tool is selected to program/debug the application.
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar.
  • Follow the steps in Running the Demo section below.
Note:
  • Windows OS has a maximum path length of 260 characters and a command-line limitation for Windows OS of 8191 characters. For details, see Path, File and Folder Name Restrictions section in MPLAB® X IDE User’s Guide.
  • The TrustZone based project come with long path name, hence the project build may fail due to exceeding Windows maximum path length.
  • Workaround: Move the project folder to C:/ drive to reduce the project path length then open in MPLAB X IDE to build the project.

Running the Demo

  • Upon completion of programming, the user should see the QT3 keypad light up and go back to sleep.
  • Activate the touchpad using the palm.
  • Select a user and enter the default passkey '12345' to open the deadbolt.
Note: This shows a custom passkey being entered. By default all users (2, 3, 4 and 5) have the same passkey - '12345'.

Reference

Comments