3.4.1 TrustZone Getting Started on PIC32CM LS00 Curiosity Pro Evaluation Kit
Description
-
The application includes Basic and Extended functionalites.
-
Basic application
- The Secure mode application toggles an LED (LED0 toggles when the switch SW0 is pressed) on a timeout basis and the periodicity of the timeout will change from 500 milliseconds to one second, two seconds, four seconds, and back to 500 milliseconds every time the user presses the switch SW0 on the PIC32CM LS00 Curiosity Pro Evaluation Kit.
- The Non-secure application requests the Secure mode application, reads the LED toggling rate and prints on the serial terminal. The LED toggling rate data is transferred to the Non-secure mode application when it requests to Secure application through Non-Secure Callables (NSC).
-
Extended application
-
The Secure mode application reads the current room temperature from the temperature sensor on the I/O1 Xplained Pro Extension Kit every 500 milliseconds. Further, the application writes the temperature readings to EEPROM and reads when a request is received from the Non-secure mode application. Also, a green LED (LED0) is toggled every time the temperature display request is received from the Non-secure mode application. The periodicity of the temperature values reading can be changed to 1 second, 2 seconds, 4 seconds, and back to 500 milliseconds whenever the user presses the switch SW0 on the PIC32CM LS00 Curiosity Pro Evaluation Kit. The temperature readings are transferred to the Non-secure mode application when it requests to Secure application through Non-Secure Callables (NSC).
-
The Non-secure mode application requests the Secure mode application the temperature values and prints them on a serial console once it receives from the Secure mode application. Further, when it gets a request from the user (in the form of a key press on the serial console), it will request the Secure mode application to retrieve the last five stored temperature values in the EEPROM. The Non-secure application prints the last five stored temperature values on the console. Also, a red LED (LED1) is toggled every time the temperature values are read from EEPROM.
-
Modules/Technology Used
- Peripheral Modules
- Secure PORT Pins (All pins by default are secure)
- Secure I2C
- Secure RTC
- Secure EIC
- Non-secure USART
- Non-secure DMAC
- Non-secure PORT Pins (USART Pins only)
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest for Secure and NonSecure projects present in harmony-manifest-success.yml under the project folder firmware/{Secure or NonSecure}/firmware/src/config/pic32cm_ls00_cpro.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Hardware Setup 1
- The PIC32CM LS00 Curiosity Pro Evaluation Kit allows the Embedded Debugger (EDBG) to be used for debugging.
- Connect the Type-A male to Micro-B
USB cable to Micro-B DEBUG USB port (J300) to power and debug the PIC32CM LS00
Curiosity Pro Evaluation Kit.
- The PIC32CM LS00 Curiosity Pro Evaluation Kit allows the Embedded Debugger (EDBG) to be used for debugging. Connect the Type-A male to micro-B USB cable to the micro-B DEBUG USB port to power and debug the PIC32CM LS00 Curiosity Pro Evaluation Kit.
Hardware Setup 2
- The PIC32CM LS00 Curiosity Pro Evaluation Kit allows the Embedded Debugger (EDBG) to be used for debugging.
- Connect the Type-A male to Micro-B USB cable to Micro-B DEBUG USB port (J300) to power and debug the PIC32CM LS00 Curiosity Pro Evaluation Kit.
- To test the extended functionality,
connect the I/O1 Xplained Pro Extension Kit to the
extension header EXT1 (J601) on the PIC32CM LS00 Curiosity Pro Evaluation Kit.
TrustZone Application Development Use Cases
-
There are two use cases:
- Single Developer (This application demonstrates a single developer use case)
- Dual Developer
- Single Developer
- A single developer develops both Secure and Non-Secure applications.
- The following steps are
automatically taken care of by the MCC.
- MCC generates both Secure
and Non-Secure projects and Sets the Secure project as a loadable project
to the Non-Secure project.
- Configures the Secure
project to generate the veneer library in the Non-Secure project path
(NonSecure/firmware/tz_pic32cm_ls00_cpro_NonSecure.X/tz_pic32cm_ls00_cpro_Secure_sg_veneer.lib).
- Configures the Non-Secure
project to link the veneer library.
- MCC generates both Secure
and Non-Secure projects and Sets the Secure project as a loadable project
to the Non-Secure project.
- Dual Developer
- The dual developer use case involves two developers.
- Initially, Developer A is
responsible for developing the Secure application; then, Developer B is
responsible for developing the Non-Secure application.
- Refer Comments for more details on the Dual Developer Application Development Use Case.
Programming Methods
- The device can be programmed in two
ways
- Refer Method 1: Programming using the prebuilt hex file.
- Refer Method 2: Programming by opening and building the application project.
Method 1: Steps for Programming prebuilt hex file
- The TrustZone project will have Secure and Non-Secure pre-built hex files.
- Program Secure hex file first followed by the Non-Secure hex file.
- The following are the steps to program these hex files.
- Download and extract the project, if not done already.
- Open MPLAB X IDE.
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt tz_pic32cm_ls00_cpro_Secure.X.production.hex file from project path pic32cm_ls00_cpro_tz_getting_started/hex.
- Select Device as PIC32CM5164LS00100.
- Ensure PIC32CM LS00 Curiosity Pro is selected under Hardware Tool and click on Next button.
- Select Project Name and
Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- Once the project opens, set the
tz_pic32cm_ls00_cpro_Secure.X.prebuilt project as Main Project by
right clicking on the project.
- Go to project properties and set
Program Options under EDBG categories to erase and program only Secure memory
region.
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Go to File -> Import -> Hex/ELF File
- In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt tz_pic32cm_ls00_cpro_NonSecure.X.production.hex file from project path pic32cm_ls00_cpro_tz_getting_started/hex.
- Select Device as PIC32CM5164LS00100.
- Ensure PIC32CM LS00 Curiosity Pro is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- Once the project opens, set the
tz_pic32cm_ls00_cpro_NonSecure.X.prebuilt project as Main Project by
right clicking on the project.
- In the
tz_pic32cm_ls00_cpro_NonSecure.X.prebuilt project, right click on Loadables
folder and click on Add Loadable File to add Secure Gateway veneer library as
shown below.
- Select
tz_pic32cm_ls00_cpro_Secure_sg_veneer.lib veneer library.
- Expand Loadables folder to confirm
that the veneer library is added to the Non-Secure project.
- Go to project properties and set
Program Options under EDBG categories to erase and program only Non-Secure memory
region.
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Method 2: Programming/Debugging Application Project
- The Trustzone project can be opened
in two ways.
- Procedure 1
- Open MPLAB X IDE.
- Close all existing projects in IDE (if any project is opened).
- Go to File -> Open Project.
- Go to reference_apps
repo path and navigate to following path
<reference_apps_path>/apps/pic32cm_ls00_curiosity_pro/pic32cm_ls00_cpro_tz_getting_started
. - Select firmware folder, enable Open Required Projects and click on Open Project button.
- Once the project opens, set
the tz_pic32cm_ls00_cpro_NonSecure project as Main Project by
right clicking on the project.
- Procedure 2
- Open MPLAB X IDE.
- Close all existing projects in IDE (if any project is opened).
- Open the project
(../pic32cm_ls00_cpro_tz_getting_started/firmware/NonSecure/firmware/tz_pic32cm_ls00_cpro_NonSecure.X)
in MPLAB X IDE.
- Ensure PIC32CM LS00 Curiosity Pro is selected as hardware tool to program/debug the application.
- Build the code and program the device by clicking on the "Make and Program Device" button in MPLAB X IDE tool bar.
- Follow the steps in Running the Demo section below.Note:
- Windows OS has a maximum path length of 260 characters and a command-line limitation for Windows OS of 8191 characters. For details, see Path, File and Folder Name Restrictions section in MPLAB X IDE User´s Guide.
- The TrustZone based project come with long path name, hence the project build may fail due to exceeding Windows maximum path length.
- Workaround: Move the project folder to C:/ drive to reduce the project path length then open in MPLAB X IDE to build the project.
- Procedure 1
Running the Demo
- Basic Functionality
- Perform Hardware Setup 1 steps mentioned above, if not done already.
- Open the Tera Term terminal application on the PC (from the Windows® Start menu by pressing the Start button).
- Set the baud rate to 115200.
- Reset or power cycle the device. LED0 toggles for every 500 milliseconds during power cycle.
- An LED (LED0) on the PIC32CM LS00 Curiosity Pro Evaluation Kit toggles on every timeout basis and the default periodicity of the timeout is 500 milliseconds.
- And also, the LED toggling rate is displayed on the serial terminal.
- Press the switch SW0 on the PIC32CM LS00 Curiosity Pro Evaluation Kit to change the periodicity of the timeout to one second.
- Every subsequent pressing of the switch SW0 on the PIC32CM LS00 Curiosity Pro Evaluation Kit changes the periodicity of the timeout to 2 seconds, 4 seconds, 500 milliseconds, and back to 1 second in cyclic order.
- See the following figure for the output.
- Extended Functionality using I/O1 Xplained Pro Extension Kit
- Perform Hardware Setup 2 steps mentioned above, if not done already.
- Open the Tera Term terminal application on the PC (from the Windows® Start menu by pressing the Start button)
- Change the baud rate to 115200.
- Press SW1 to start the running the extended functionality.
- The temperature values (in °F)
are displayed on the terminal every 500 milliseconds, as shown below:
- Also, notice the LED0 blinking at 500 millisecond rate.
- The temperature may be varied by
placing the finger on the temperature sensor (for a few seconds).
- Press the switch SW0 on PIC32CM
LS00 Curiosity Pro Evaluation Kit to change the default sampling rate to 1 second.
- Every subsequent pressing of
switch SW0 on PIC32CM LS00 Curiosity Pro Evaluation Kit changes the default
sampling rate to 2 seconds, 4 seconds, and 500 ms and back to 1 second in cyclic
order as shown below.
- While the temperature sampling rate changes on every switch SW0 press, notice the LED0 toggling at the same sampling rate.
- Press any character on the
terminal to display the last five values written to the EEPROM. Notice that a red
LED (LED1) will be toggled when a key is pressed in the serial console to read the
temperature values from the secure EEPROM.
- Anytime press SW1 to start running basic functionality shown in Basic Functionality.
Comments
- Getting Started with the PIC32CM LE00/LS00/LS60 Curiosity Pro Board (DS00004511)
- Dual Developer Application Development Use Case with
TrustZone on SAM L11 Using MPLAB Harmony v3 (DS90003306)Note: Though this technical brief is on SAM L11 MCUs, the TrustZone concepts it describes also applies to PIC32CM MC LS00 MCUs.
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project