3.9.2 Software Attack Protection Application on PIC32CM LS00 Curiosity Nano + Touch Evaluation Kit
Description
This application demonstrates safeguarding the PIC32CM LS00 MCU against software attacks using the PIC32CM LS00 Curiosity Nano + Touch evaluation kit.
- By leveraging the Boot ROM’s Secure Hash Algorithm 2 (SHA-256) Authentication, the
PIC32CM LS00 can identify unauthorized code fragments in the Non-Secure Memory and
replace them with an authentic version of the Non-Secure firmware.
Modules/Technology Used
-
Peripheral Modules
- SERCOM3 (USART)
- RTC
- EIC
- SYSTICK
- Power Manager (PM)
- EVSYS
- NVMCTRL
- PORT
-
System Services
- STDIO
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer to the Project Manifest present in
harmony-manifest-success.yml under the project folder
firmware/src/config/default.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version. Alternatively, click here.
Due to Microchip regularly update tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB® Harmony v3 Project Manifest Feature (DS90003305).
Hardware Setup
- Connect the PIC32CM LS00 Curiosity Nano
+ Touch evaluation kit to the host PC as a USB device through a Type-A male to micro-B
USB cable connected to Micro-B USB (Debug USB) port
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to
File>Import>Hex/ELF File - In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CM5164LS00048
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section
Programming/Debugging Application Project
- Open the project group
(
pic32cm_ls00_software_attack_protection/firmware/tz_pic32cm_ls00_cnanogroup) in MPLAB X IDE - Right click on
tz_pic32cm_ls00_cnanogroupfile and go toOpen Required projects>Open All Projects - Then, right click on the non-secure project and click Set as Main Project
- Ensure
PIC32CM LS00 Curiosity Nanois selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section
Running the Demo
- After building the application and
completing the programming, open the MPLAB Data Visualizer by clicking the highlighted
icon below.

- Configure the serial port setup of the
PIC32CM LS00 Curiosity Nano + Touch evaluation kit by clicking the Gear icon shown
below.

- Set the 115200 as baud rate in the COM
setting.
- Open the Serial Port of the PIC32CM LS00
Curiosity Nano + Touch evaluation kit by clicking the Play icon as follows.

- Select the Sent to Terminal to view the
serial console message and click Close.
- Open the command prompt and navigate the
following location.
Path:
C:/Program Files/Microchip/MPLABX/v6.20/mplab_platform/mplab_ipeImportant: The PIC32CM LS00 Curiosity Nano + Touch evaluation kit has no RESET button to reset the MCU. To reboot the board, the RESET command is sent to the nEDBG to reset the MCU with the help of MPLAB IPECMD. - Run the following command to reset the
PIC32CM LS00 Curiosity Nano + Touch evaluation kit.
ipecmd.exe -P32CM5164LS00048 -TPNEDBG -OK - Observe the start-up console message on
the MPLAB Data Visualizer and the LED1 will toggle on the PIC32CM LS00 Curiosity Nano +
Touch evaluation kit.
- Press the switch SW1 on the PIC32CM LS00
Curiosity Nano + Touch evaluation kit to simulate a software attack.
- Observe the console message of software
attack initiation on the MPLAB Data Visualizer.
Comments
- Reference Training Module: Arm TrustZone Getting Started Application on PIC32CM LS60 (Arm Cortex-M23) MCUs
- This application demo builds and works
out of box by following the instructions in Running the Demo section. If the user needs to
enhance/customize this application demo, should use the MPLAB Harmony v3 Software
framework. Refer to the following links to setup and build the applications using MPLAB
Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project